You are here: Technical References > System Library

System Library

Name Description
PrintMessage Generate an output message in the log windows.
GetCtrlErrors Get a list of the active errors and alarms on the controller.
ClearCtrlErrors Clears the list of active errors and alarms on the controller.
GetCtrlPerf Generate a text file with performance statistics of the controller.
GetCtrlInfo Get the serial, model, and/or part number of the controller.

Table 11-52: List of System Functions

 

Print Message

GetCtrlErrors

ClearCtrlErrors

GetCtrlInfo

GetCtrlPerf


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™